Diodes Incorporated

Pericom Expands Its Timing Portfolio to Support 25/40/100Gb Ethernet Applications

Pericom Semiconductor Corporation (now a part of Diodes Incorporated) (NASDAQ: DIOD), a leading supplier of serial high-speed switching, connectivity, signal-integrity and timing solutions, today announced the industry's complete timing solution for fast growing 25/40/100GbE applications with ultra low jitter crystal oscillators, FlexOut clock generators, and high performance buffer families.

A huge growth in always-on mobile devices, the explosion in cloud computing and other needs for high volume data traffic are driving the needs of higher data throughput for networking equipment. The mainstream 10GbE backbone interface is being upgraded to higher speed interfaces such as 25/40/100GbE to increase the data throughput of network backbones for networking and data centers. Chipsets that support these higher backbone data rates require even lower jitter, more stable clock sources that can be low enough to provide system engineers with design margin. Ultra low jitter clock source is the key to the high speed interface for system performance.

"Pericom has the best performance solutions that can achieve sub 100 femto-second (fs) jitter performance to provide system design margins for high data rate applications," said Wendy Zhou, product marketing director, Pericom Semiconductor. "The modern system design needs to support various clock tree architectures. Our complete solutions provide multiple Ultra low jitter clock tree implementation options for system engineers to meet the performance, board space, and cost requirements."

Complete timing solutions from Pericom include crystal, crystal oscillator (XO), clock synthesizer, and clock buffers for growing 25/40/100GbE applications. These products are an important part of Pericom's timing solution targeted for the fast growing, Networking/Data Center segment:

Ultra Low Jitter XO - UX Family

  • Phase jitter as low as < 100fs
  • Support CMOS and differential outputs

FlexOut Ultra Low Jitter Clock Generator - PI6CXG06F62a

  • Up to 6 differential outputs
  • Phase jitter as low as 80fs

High Performance Differential and Single-Ended Buffers

  • Up to 10 outputs
  • Up to 6GHz speed
  • Additive jitter as low as 30fs

Pricing & Availability

The UX Family, FlexOut Clock Generator, and High Performance Buffers are available in production quantities. Additional information and a volume pricing quote is available from Pericom worldwide sales, or by requesting a specific product price quote on www.diodes.com.

The complete timing portfolio is available here

About Pericom:

Pericom Semiconductor Corporation enables serial connectivity with complete solutions for computing, communications and consumer market segments. Pericom's integrated circuits (IC) and frequency control products (FCP) provide the connectivity, timing, switching, bridging and signal conditioning of high-speed signals required by today's electronic applications. Pericom is based in Milpitas, California, with design centers and technical sales and support offices around the world. Pericom is a qualified supplier to more than 100 of the world's largest (Tier 1) corporations. Pericom was acquired by Diodes Incorporated (NASDAQ: DIOD). Learn more at www.diodes.com.