Diodes Incorporated

Diodes Incorporated Increases Performance of Schottky Diodes by as Much as 20%

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, today introduced the SDT series of Schottky diodes. Using an advanced deep-trench process, these devices deliver superior performance at similar or lower cost to planar-type Schottky diodes. The initial family of 29 devices, housed in thermally-efficient packages, provides the blocking, free-wheeling, flyback and other diode functions commonly found in a wide range of applications, such as AC-DC chargers/adapters, DC-DC up/down conversion, and AC LED lighting.

Diodes’ innovative deep-trench process enables the SDT series of Schottky diodes to achieve a forward voltage (VF) as low as 0.62V along with a leakage current of just 3.5µA. This exceptional performance results in outstanding power efficiency and contributes to smaller form-factors for end-system designs. Within the family, maximum average rectified current ratings from 5A to 40A are offered, with peak repetitive reverse voltages (VRRM) up to 120V and forward surge currents (IFSM) as high as 280A, ensuring robust system operation across the full temperature range.

PowerDI®5, TO220AB, and ITO220AB package options all offer excellent thermal transfer properties that allow the SDT series Schottky diodes to perform reliably in demanding applications. These packages are well-suited for high-volume manufacturing and also allow the SDT parts to be used as drop-in replacements for generic planar-type Schottky diodes. Further information is also be available at www.diodes.com.

PowerDI is a registered trademark of Diodes Incorporated.

Related Files