Diodes Incorporated (Nasdaq: DIOD) introduces the industry’s first ReDriver™ to reach PCI Express® (PCIe®) 6.0 protocol speeds (up to 64 GT/s) while being backwards-compatible with PCIe 5.0/4.0/3.0 protocols. The PI3EQX64904 is a low-power, high-performance, 64GT/s, four-differential-channel, PAM4, linear ReDriver. Target applications include AI data centers (storage and servers), workstations, 5G networking, CPU-to-network (PCIe NIC card) and CPU-to-storage (NVME) interconnects, and CPU-to-CPU interconnects within high-performance computing (HPC) clusters.
The PI3EQX64904 ReDriver provides optimized linear equalization with tunable low-frequency and high-frequency zeros at the equalizer stage to boost the PAM4 signal quality of high-speed PCIe interfaces. It optimizes performance over a variety of physical media by reducing intersymbol interference, correcting for known channel losses at the transmitter, and restoring signal integrity at the receiver. This results in an improved eye pattern at the receiver with the margins required to deliver reliable PCIe communications at 64GT/s PAM4 with low bit error rates (BER).
The PI3EQX64904 meets the Modern Standby mode requirements outlined by Microsoft Corporation of consuming less than 5mW of power when the system is in PCIe L.1.2 deep standby mode. The device also delivers elevated linearity and ultra-low jitter characteristics. Linear ReDrivers are commonly used to achieve PCB trace extension while minimizing cost and power consumption. They can also deliver lower latency.
Requiring a supply voltage of 3.3V ±0.3V, the PI3EQX64904 ReDriver can operate over an industrial temperature range of -40°C to +85°C. The device is offered in a 31-contact W-LGA-31L (6.1mm x 2.7mm) package and is priced at $5.00 each in 3,000-piece quantities.
Diodes will be showcasing this new product at the PCI-SIG® Developers Conference, booth #11.
For further information on how ReDrivers can improve signal integrity, please visit: https://www.diodes.com/products/connectivity/signal-integrity-redriversrepeaterssignal-conditioners/#
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. We leverage our expanded product portfolio of analog and discrete power solutions combined with leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific products and solutions-focused sales, coupled with global operations including engineering, testing, manufacturing, and customer service, enable us to be a premier provider for high-volume, high-growth markets. For more information, visit www.diodes.com.
PCI-SIG®, PCI Express®, PCIe® and CopprLink™ are registered or unregistered trademarks of PCI-SIG in the United States and other countries. All rights reserved.
ReDriver is a trademark of Diodes Incorporated.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
All other trademarks are the property of their respective owners.
© 2025 Diodes Incorporated. All Rights Reserved.
Company Contact:
Gurmeet Dhaliwal
Director, Investor Relations & Corporate Marketing
Diodes Incorporated
+1 408-232-9003