Diodes Menu Close
Diodes Pericom: A product line of Diodes Incorporated
Back to Press Releases

Diodes Incorporated Introduces World’s First Power Switch to Fully Support USB Type-C Power Delivery and Hot-Swap Operation

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, today introduced the DPS1133. This single-channel power switch is the world’s first high-voltage power switch designed to meet all the demanding protection and fast-role swap requirements of USB Type-C™ ports. As such, it addresses the full gamut of mobile and desktop computing devices and peripherals, and numerous other applications in the consumer electronics, mobile communications, industrial, and medical markets, such as smartphones, AR/VR goggles, robotics, automotive infotainment, and home electronics.

Specifically, the DPS1133 protects the VBUS lines to and from USB Type-C connectors, meets the fast role swap (FRS) timing criteria defined by the latest Release 3.0 Power Delivery Specification, and supports all the allowed USB-C port operational modes: downstream facing (DFP), upstream facing (UFP), and dual-role (DRP). Designed to operate between 4.5V and 24V, the DPS1133 can either act to provision or consume power at up to 3.5A through a USB Type-C connector, automatically protecting and recovering from fault conditions like over-voltage, over-current, short-circuit, reverse-voltage, and over-temperature, without the intervention of a system controller.

The low on-state resistance of the DPS1133 power switch (typically ≤30mΩ) enables the 3.5A maximum continuous current and helps minimize power dissipation, while the thermally efficient QFN4040-17 package ensures a sufficiently low surface temperature during operation. Usability is enhanced through the ability to use external resistors to adjust many device parameters, such as voltage and current limits, and ramp times. Control pins also allow the input and output ports to be discharged through an internal resistor.Further information is also be available at www.diodes.com.

USB Type-C is a trademark of USB Implementers Forum.

Related Files

Web Analytics