Diodes Incorporated

Ultra-Low-Current LDO from Diodes Incorporated Handles Loads up to 150mA with 1% Accuracy

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, today introduced the AP7350. This low dropout voltage regulator (LDO) is available with output voltages from 1.2V to 3.3V, supporting load currents up to 150mA. The AP7350 targets low-power, handheld and wearable device applications. Its ultra-low quiescent current of just 0.25μA and 1% accuracy enable designs to achieve extended battery life while a chip scale package just 0.64mm square occupies the smallest possible board space.

The design of the AP7350 LDO recognizes two of the key requirements inherent in the multitude of new sensing applications that are contributing to growth of the Internet of Things (IoT). These are the need for low power consumption, since many devices will be battery-powered, and small size, to fit the often-constrained form factor designs typified by wearable devices. With a quiescent current of 0.25μA and a typical standby current of 20nA the AP7350 LDO enables low sampling rate system designs that can operate for years on a single coin cell battery. The miniature chip-scale package is between a quarter and half the size of competitive solutions, and has a low profile of just 0.34mm.

The AP7350 is offered with seven output voltages: 1.2V, 1.5V, 1.8V 2.5V, 2.8V, 3.0V, and 3.3V. These address the voltage rail requirements of microcontroller, FPGA, other digital and analog ICs, and sensor circuits commonly found in low-power IoT applications. Output accuracy is 1% at room temperature and 1.5% over the full -40°C to +85°C operating temperature range. Further information is also be available at www.diodes.com.

Related Files