Ten of the most common logic functions have initially been introduced: Quad 2- input AND, NAND, NAND with Schmitt trigger inputs, OR and XOR gates, along with 3 different types of hex inverter and a hex buffer with open drains. Running off a wide 2.0V to 5.5V supply range, Diodes' 74LV parts will support both mini, cell-backed portable and traditional 5V applications.
With an optimized drive capability, typically delivering 12mA at 4.5V, the 74LV logic provides a stronger, faster switching output than the older 74HC or 74AHC parts. In addition, IOFF output circuitry is a design feature across the family, disabling devices when powered down, to prevent exposure to harmful back currents.
Inputs are also 5.5V tolerant, enabling the logic devices to operate comfortably in voltage translations duties. And drawing less than 1μA in many applications, the 74LV parts will meet the requirements of a variety of energy-sensitive circuit designs.
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes' corporate headquarters, logistics center, and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes' wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two more located in Shanghai, China. In addition, two assembly-test facilities are located in Shanghai; two are located in Chengdu, China, with one in Neuhaus and one in Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Fort Worth, Texas; Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; Suwon, South Korea; Tokyo, Japan; and Munich, Germany, with support offices throughout the world. For further information, including SEC filings, visit Diodes' website at www.diodes.com.
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-987-3900
E: pressinquiries@diodes.com
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com