Diodes Menu Close
Diodes Pericom: A product line of Diodes Incorporated

PCIe 封包交換器

PCIe Switch

Diodes 的 PCI Express 解決方案以穩固的 PCI-X 產品為建構基礎,支援訊號品質、系統效能、彈性、可靠性、系統時脈、EMI 及 Express 纜線等應用。

Diodes 的 PCI Express 封包交換器具備低延遲、低功耗且完全相容(PCISIG 2.1 和 1.1)的特性,支援多重 I/O 裝置和主機裝置 (root complex) 或微處理器之間的高速點對點 (point-to-point) 串接以進行最佳整合,以及通往主機之端點流量的扇出或點對點 (peer-to-peer) 通訊,是工業電腦網路儲存以及行動桌上型電腦的最佳選擇。


相關連結

Time to switch button

 

PCIe 封包交換器 Details

Key Features:

  • Up to 5-ports, 8-lanes; most cost effective switch family in the market
  • Supports isochronous data streaming: real-time/live video
  • 8 traffic classes and 2 virtual channels per port
  • Customer programmable switching and EEPROM configurable
  • Customer programmable PHY and switching parameters (cut through or store/forward mode)
  • Very low-power shut-off features
  • Smallest package in industry (PI7C9X20404GP)

PCIe 封包交換器 FAQs

Can I change Pericom packet switch's PHY parameters by EEPROM or SMBus?

Yes, all Pericom's packet switches provide EEPROM/SMBus to change PHY parameters including Low Driver Current, High Drive Current, Driver Transmit Current, De-emphasis Transmit Equalization, Receive Termination Adjustment, Transmit Termination Adjustment and Receiver Equalization Level Control.

Can I change Pericom packet switch's PHY parameters by strapping pin options?

Only GreenPacket Family packet switches, PI7C9X20505GP, PI7C9X20508GP, provide strapping pin option to change PHY parameters to improve signal quality. The following strapping pins are available: HIDRV, LODRV, DTX[3:0], DEQ[3:0], RXEQCTL[1:0], RXTERMADJ[1:0] and TXTERMADJ[1:0].

Do Pericom's packet switches accept reference clock source which is different from the root complex?

Yes, Pericom Packet Switches support operation in asynchronous mode, in which the reference clock source of Pericom packet switch is different from that of the root complex. However, the deviation in the clock signals must be within +/- 300ppm.

Do Pericom's packet switches require the device driver?

Yes, Pericom's Packet Switches require the standard PCI-to-PCI Bridge device driver in order to work, which is built in most of the OS's. That is, most of the OS's automatically install the standard PCI-to-PCI Bridge device driver when a Pericom's packet switch is plugged in the system for first time.

Do Pericom's Packet Switches Support Industrial Temperature Range (-40oC to +85oC)?

"YES, please refer to the following application notes.

AN219 – GreenPacket PCI Express Packet Switch – Industrial Temperature Support 1.0

AN220 – PI7C9X20303SL-404SL Industrial Temperature Support

AN221 – PI7C9X20303ULA Industrial Temperature Support"

 

Does Pericom provide a Compatibility Test List for the Packet Switches?

Yes.  Please refer to the Application Note, "AN227 – Product Compatibility List" for the complete list.

Does Pericom provide the design kits for packet switches and what information is included in the kit?

Yes, Design Kits for Packet Switches are available and include datasheet, product brief, reference schematics, software tools, demo board user manual, design guideline, IBIS file and related application notes. The design kits can be requested from your distributer or Pericom FAE.

Does Pericom provide the power consumption for the Packet Switches?

Yes, power consumption information is included in the design kit.

Does Pericom's packet switches support Hot-Plug feature?

GreenPacket Family (PI7C9X20505GP, PI7C9X20508GP) provides full support for hot plug functions, including Power Indicator, Attention Indicator, Attention Button, Presence Detected Changes, Slot Power Enable Power Fault.  SlimPacket Family (PI7C9X20303SL, PI7C9X20404SL) and UltraLo Family PI7C9X20303UL only support Presence Detected Changes event.  EEPROM or the strapping pins are used to enable the hot plug feature.

Does Pericom's packet switches support Spread Spectrum Clock (SSC) Sources?

No, Pericom packet switch does not support SSC sources.

How do I configure the configuration registers of Pericom's packet switches?

Pericom's packet switches can be configured by the configuration registers. There are three methods for this purpose: configuration read/write, SMBus, and EEPROM. Configuration read/write and SMBus can access configuration registers on-line. However, SMBus can only access these registers below 100H offset. Configuration read/write method is required if you intend to access registers above 100H offset. EEPROM can change the default values of certain configuration registers. EEPROM content is auto-loaded to packet switch when power-on.

How do I use SMBUS interface of Pericom's packet switches?

Please refer to the application note, "PCIe Packet Switch SMBus Programming Guild 0.1c" for detailed information. Please set SMBus address using GPIO[7:5]. Otherwise, SMBus may not work due to unknown SMBus address.

How to implement MRL_PDCx/PRSNTx pin?

The pin is name "MRL_PDCx" in GreenPacket Family packet switches and "PRSNTx" in SlimPacket Family and UltraLo Family with the same function. MRL_PDCx/PRSNTx pin is used to indicate whether a device is present in the slot of downstream ports in express card interface implemention. When MRL_PDCx/PRSNTx is asserted high, it represents the device is present in the slot of downstream ports. Otherwise, it represents the absence of the device. If express card interface is not implemented, MRL_PDCx/PRSNTx should be connected to GND through a pull-down resistor.

Is EEPROM required in the implementation?

The implementation of EEPROM depends on specific application. Normally, a packet switch is fully functional without EEPROM. However, in certain applications, EEPROM is needed to change certain default values of configuration registers. We recommend keeping the EEPROM footprint and circuitry just in case.

Is there a replacement for an obsolete part?

Not all obsolete parts will have a direct replacement. However, we recommended that you contact your regional sales office.

What are the PHY parameters?

In order to meet the different application needs, the driving current and equalization of each transmitting channels can be adjusted individually using strapped pins (GreenPacket Family) and EEPROM (GreenPacket/SlimPacket/UltraLo Family). The driver current of each channel is set to 20mA in default mode without pins being strapped. To change the current value, the user can strap the pins/EEPROM either for nominal value (HIDRV, LODRV) or actual value (DTX [3:0]), which is a scaled multiple of Inom. The following tables illustrate the possible transmitted current values the chip provides.

What are the reasons that a Pericom's packet switch can not detect the plugging in of an endpoint in embedded system?

It is most likely that the boot code of the embedded system does not initialize Pericom's packet switch. The packet switch needs to be initialized in order to work normally. The packet switch is initialized by BIOS on x 86 systems and by the boot code on embedded system.

What are the reasons that Pericom's packet switch on an evaluation board can not detect an express card or a mini-pcie device?

The evaluation board of a Pericom's packet switch only provides the PCIe x1 slot on the downstream ports. Customers need an adapter they would like to plug in the express card or mini-pcie device. When the PRSNT# pin of the adapter is floating, the express card or mini-pcie card can not be detected.

What are the types of jitter?

There are several types of jitter, but the main ones are: cycle-to-cycle jitter, period jitter, half period jitter, and peak-to-peak jitter. Jitter terminology can be found in AB36: Jitter Measurement Techniques at Application Brief No. 36 or Application Note No. 27.

What is Surprise Hot Removal Function? Do Pericom's packet switches support it?

Surprise Hot Removal function allows unplugging of express card without prior notification. All Pericom's packet switches support this function. All downstream ports of SlimPacket Family and UltraLo Family packet switches support the surprise hot removal function. Only Port 1 and Port 2 of GreenPacket Family packet switches support this function. That is, only Port 1 and Port 2 of GreenPacket Family packet switches can implement the express card interface.

What is the lead finish for Pericom products? What about lead-free?

All Pericom's products that are not lead-free are composed of 85% Sn and 15% Pb. For lead-free products, they are composed of 100% matte Sn. Lead-free products are marked and ordered with the letter "E" suffix at the end of the part number.

What is the requirement of the reference clock of Pericom's packet switches?

The reference clock DC specifications and AC timing requirements are shown in the table below. More details can be found in "PCI Express Card Electromechanical Specification Revision 1.1", Chap 2.1.3.

 

Where can I find Mean Time Before Failure (MTBF) or Failures In Time (FIT) values for Pericom products?

FIT and MTBF data can be found at Pericom's Quality webpage.

Where can I find the information on your Pb-free and "Green" packaging?

Lead (Pb)-Free and Green information can be found on individual datasheets or Pb-Free & Green Page.

Why is AC-Coupling required in the reference clock input pairs?

The reference clock input pins connect to external 100MHz differential clock. The signal must match to LVPECL or HCSL spec.  A 100nF capacitor should be placed between the clock source and the packet switch. The purpose of this capacitor is to achieve AC coupling. This AC Coupling ensures the Packet Switch is compatible with the differential clock signals regardless the type of the clock. The input clock signals must be delivered to the clock buffer cell through an AC-coupled interface so that only the AC information of the clock is received, converted, and buffered. Please refer to the application note, "Express Interface AC-Coupling Application Note", in the design kit for more details.