Diodes Incorporated (Nasdaq: DIOD) today introduces its first automotive-compliant* 3D linear Hall effect sensor. The AH4930Q detects the magnetic field in the X, Y, and Z directions, allowing for reliable and high-precision contactless rotary motion and proximity detection. Applications include rotary and push selectors on infotainment systems, stalk gear shifters, door handles and locks, and powered seat adjusters.
The AH4930Q integrates a 12-bit temperature sensor for accurate on-chip compensation. Its robust signal path and 12-bit data converter via ADC provide high resolution for each measurement direction down to 1 Gauss (0.1mT) per bit for precise positional accuracy. The implemented I2C interface enables seamless communication for measurement data reading and runtime programming with host systems as fast as 1Mbps to support real-time adjustments.
The device has three operating modes plus a power-down mode where it consumes only 9nA. Its three operating modes provide a power consumption-data acquisition compromise, including an ultra-low-power mode consuming only 13µA (10Hz), to its fast-sampling mode of 3.8mA (3.3kHz) for constant measurement functionality. With a 10µs wake-up time, 4µs response time, and wide bandwidth, the AH4930Q delivers ultra-fast data acquisition even for the most demanding applications.
The AH4930Q operates on supply voltages from 2.8V to 5.5V, and a temperature range from -40°C to +125°C. The 3D linear Hall effect sensor is housed in the industry-standard 6-pin SOT26 (Type A1) package and is available at $0.50 for 1,000-piece quantities. A standard-compliance version, the AH4930, is also available for industrial and commercial applications.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. We leverage our expanded product portfolio of analog and discrete power solutions combined with leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific products and solutions-focused sales, coupled with global operations including engineering, testing, manufacturing, and customer service, enable us to be a premier provider for high-volume, high-growth markets. For more information, visit www.diodes.com.
*Automotive-compliant—qualified to AEC-Q100 Grade 1, manufactured in facilities certified to IATF 16949, supporting PPAP documents.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
All other trademarks are the property of their respective owners.
© 2025 Diodes Incorporated. All Rights Reserved.
Company Contact:
Gurmeet Dhaliwal
Director, Investor Relations & Corporate Marketing
Diodes Incorporated
+1 408-232-9003